- Honeywell Selected By Lockheed Martin Sikorsky-Boeing To Power DEFIANT X Helicopter In Key U.S. Army Pursuit
Honeywell Selected By Lockheed Martin Sikorsky-Boeing To Power DEFIANT X Helicopter In Key U.S. Army Pursuit
New HTS7500 turboshaft engine provides the most favorable power-to-weight ratio and total value in its class of military helicopter turboshaft engines
February 10, 2022
PHOENIX, Feb. 10, 2022 /PRNewswire/ -- Honeywell (NASDAQ: HON) has been selected to provide its new HTS7500 turboshaft engine as the power behind the Lockheed Martin Sikorsky-Boeing DEFIANT X® helicopter, currently a contender to win the U.S. Army's Future Long-Range Assault Aircraft (FLRAA) competition.
The HTS7500 turboshaft engine is the newest and most technologically advanced model in Honeywell's family of military engines, which includes the iconic T55 engine that has powered the H-47 fleet for over 60 years. Like the T55, the HTS7500 is a highly reliable engine designed to thrive in austere environments and to perform to keep military personnel safer. The HTS7500 enhances mission readiness and exceeds mission power and fuel consumption requirements. The new engine comes equipped with a modernized control system, which enables a highly secure flow of engine data. The control system improves operating capabilities, reduces life-cycle costs, and ensures engine health status through its digital thread road map.
"This engine builds upon the battle-proven architecture of the T55, but the HTS7500 takes engine performance, reliability and efficiency to a whole new level," said Dave Marinick, president, Engines and Power Systems, Honeywell Aerospace. "The engine is structurally similar, which is great for maintainers in the field because they can use current tools and training. However, when it comes to performance, the HTS7500 is 42% more powerful than the T55-GA-714A and has the lowest total weight compared to other engines in its horsepower class."
"We're committed to the U.S. Army's focus on modernization and multidomain operations, and the selection of Honeywell's latest engine technology for the DEFIANT X® is proof of that commitment," said Ricky Freeman, president, Defense and Space, Honeywell Aerospace. "The HTS7500 checks all the right boxes for the Lockheed Martin Sikorsky-Boeing team and the Army, and we are excited to play a part in the future of vertical lift for our Army customer and Team DEFIANT."
The DEFIANT X® will be the fastest, most maneuverable assault helicopter in history. It can fly two times faster and farther than the Black Hawk and is currently being tested in a digital combat environment, where it continues to prove its unmatched range and survivability.
FLRAA was initiated by the U.S. Army in 2019 to develop a new utility helicopter that will replace the Sikorsky UH-60 Black Hawk starting in 2030. The Black Hawk was developed in the 1960s and 1970s and was selected by the U.S. Army in 1976. FLRAA will provide the next generation of capability for decades to come for the U.S. Army, and the HTS7500 has been built to provide world-class reliability and time on wing for this next generation of aircraft.
Engines designed by Honeywell have been at the forefront of aircraft propulsion for nearly seven decades, shaping aviation's progress in civilian and military applications around the world. Honeywell's high-performance, high-power engines combine rigorous testing with rugged design, ensuring smoother operation in the harshest environments. Continuous improvement programs have resulted in engines that today provide more power with lower fuel consumption, enhanced safety and proven reliability.
For more information on Honeywell's HTS7500 turboshaft engine and its role in the FLRAA pursuit, visit aerospace.honeywell.com.
About Honeywell
Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft. The Aerospace business unit builds aircraft engines, cockpit and cabin electronics, wireless connectivity systems, mechanical components and more. Its hardware and software solutions create more fuel-efficient aircraft, more direct and on-time flights and safer skies and airports. For more information, visit www.honeywell.com/us/en or follow us at @Honeywell_Aero.
Honeywell (www.honeywell.com/us/en) is a Fortune 100 technology company that delivers industry-specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/us/en/news.
Copyright © 2025 Honeywell International Inc.