HTF7000 delivering 99.96 percent reliability
Utilizing SABER technology, new HTF7000 engines will beat current emission levels by 25 percent
GENEVA, May 17, 2011 -- Honeywell (NYSE: HON) Aerospace’s HTF7000 fleet of turbofan engines has accrued more than one million hours of operation on the Bombardier* Challenger 300* and is delivering more than 99.96 reliability for operators.
The HTF7000 exclusively powers the Bombardier Challenger 300, a super-midsize business jet capable of flying nonstop from New York to London at 0.80 Mach under certain operating conditions. There are more than three hundred Bombardier Challenger 300 aircraft in service with corporate and private operators and in Bombardier's Flexjet fractional ownership program.
“Planned with years of industry input from customer advisory boards, steering committees and surveys, along with Honeywell’s expertise in the business aviation propulsion market, the HTF7000 is one of the most reliable, fuel efficient and low-cost engines in business aviation today,” said Rob Wilson, President, Business and General Aviation, Honeywell Aerospace, a leading global provider of turbofan engines for the mid-size business jet market. “With one million hours of service and counting, the HTF7000 has a dispatch reliability rate in excess of 99.96 percent and an in-flight shut down rate of less than .004 percent. Our customers continue to be thrilled with the engine’s state-of-the-art performance and unparalleled reliability.”
Development of the HTF7000 began in 1998 to answer demand for a turbofan engine with extremely high reliability and very low operational costs. Customer interest in features such as access to all the main shaft bearings and on-wing combustors drove a significant portion of the ultimate design of the engine. The HTF7000 received FAA certification in June 2002 and JAA validation in December 2002.
“We are extremely pleased to mark this milestone on such a reliable and productive power plant for our most popular Challenger 300 business jet,” said Michel Ouellette, Vice President and General Manager, Challenger Aircraft. “Durability and performance are key requirements when first choosing an engine for one of our business aircraft platforms. The HTF7000 clearly performs to the required specifications and also is easily supported in the field by our Aircraft Service Centers.”
The HTF7000 produces approximately 7,000 pounds of thrust at takeoff, with a flat rating of 86 degrees Fahrenheit (ISA +15°C), allowing the Bombardier Challenger 300 to fly transcontinental missions up to 3,100 nautical miles (5,741 km) with eight passengers, two-crew and maximum allowable fuel under certain operating conditions.
The HTF7000 design incorporated ‘green technologies’ from the onset, including reductions in fuel burn, resulting in lower carbon dioxide emissions, reduced operational costs and best-in-class noise levels with the smallest noise footprint.
Later this year, Honeywell will incorporate improved green technology for its HTF7000 family. Honeywell’s Single Annular comBustor for Emissions Reduction (SABER) will enable emissions savings of up to 25 percent less than current levels. Fielded HTF7000’s will be able to be retrofitted with SABER technology, and it will be included in new engine deliveries for all aircraft powered by the most dependable engine in the 7,000-pound thrust class.
Honeywell’s aerospace business is a leading global provider of integrated avionics, engines, systems and service solutions for aircraft manufacturers, airlines, business and general aviation, military, space and airport operations.
Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
Honeywell and the Honeywell logo are the exclusive properties of Honeywell International, Inc., are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2011 Honeywell.
* Either registered or unregistered trademarks of Bombardier Inc. or its subsidiaries.
This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.
Media Contacts:
Bill Reavis
Honeywell Aerospace
+1 602-625-9027
bill.reavis@honeywell.com
Honeywell Aerospace Media Center
Chris Martin
Waggener Edstrom Worldwide
+44 (0)7789 280 239
cmartin@waggeneredstrom.com
Honeywell Aerospace Media Center