Press Releases
  Back to Index
3/11/2011 
Honeywell Opens The Largest School In Southeast Region Of Haiti 

 

Nine-Building, 40,000 Square Foot Complex, Will Serve More Than 600 Local Children, Rises Just Seven Months After Groundbreaking Following Devastating January 2010 Earthquake

 

JACMEL, HAITI (March 11, 2011) -- Honeywell (NYSE: HON) Chairman and CEO Dave Cote and Honeywell Hometown Solutions President Tom Buckmaster joined students, parents, teachers, school administrators, and community leaders to open Ecole Nationale Jacob Martin Henriquez, a new, state-of-the-art public school in the hard-hit city of Jacmel in southern Haiti.  The nine-building school complex will provide a new educational home and free meals to more than 600 local children in grades K through seven.

 

The school was built using contemporary, sustainable building methods and is designed to withstand any potential future earthquakes.  Honeywell used the school’s construction to train local builders in modern earthquake-resistant construction and environmentally-conscious techniques that can save Haiti money and natural resources in the years to come. Honeywell has established a scholarship fund in partnership with Operation USA to help cover the cost of books, uniforms and other student expenses.

 

“Working together with Operation USA, Mayor Edwin Zenny, and the City of Jacmel, we have delivered on our commitment to rebuild, creating a terrific community asset and environment for learning just seven months after we broke ground,” said Cote. “This is one of the largest post-quake rebuilding projects completed in Haiti so far.  Haiti’s children have been profoundly affected and we are gratified to be able to help Haiti continue their education and to play a meaningful role in improving the learning environment.”

 

Jacmel, a seaside town with a population of 80,000 and located 45 kilometers from the epicenter of the earthquake, saw an estimated 80% of its buildings either damaged or destroyed, with the most severe devastation in the poorer neighborhoods. Before its destruction, Ecole JM Henriquez – one  of the few free schools available to the city’s children – served 400 students between the ages of seven and 17.  The new school complex, which sits on one and a half acres overlooking the bay of Jacmel, will offer 600 students in grades K through seven a new, free educational home that features a computer lab, library, cafeteria, administration building, six classroom buildings, a sustainable community garden and an athletic field.

 

Immediately following the earthquake, Honeywell committed $1 million in aid to Haiti, including a 100 percent match of employee donations, to fund rebuilding projects.  Honeywell also made business jets available to relief agency Operation USA for airlift support to deliver medical supplies and transport medical staff.

 

In an effort to promote good health and nutrition while also incentivizing school enrollment and thereby enhancing literacy rates, a feeding program was developed for all students attending the school. At the core of the program are the community gardens on the school grounds. The gardens will be cultivated and maintained by the students, their families, and school staff. All produce grown in the gardens will be used in the daily meal provided to the children. These “learning gardens” will integrate practices of resource management, basic horticulture, water harvesting, composting, and small animal husbandry.

 

The government of Haiti estimates that approximately 230,000 people were killed and more than 300,000 injured in the massive January 2010 earthquake, including 38,000 students and 1,300 teachers and other education personnel. More than 4,000 schools and the Ministry of Education’s headquarters were destroyed, and all available data on education was lost. An estimated three million students are believed to have suffered an interruption to, or complete cessation of, their educations. Only 50% of the children living in resettlement camps and relocation sites attend school.


 

 

SCHOOL CONSTRUCTION FACTS:

•  Nine buildings with space for 600 students

•  40,375 square feet

•  15 classrooms

•  10 bathrooms

•  Five showers

•  20 computers

•  Average building is 4,486 square feet (largest 5,821 square feet)

•  Total construction workers employed: more than 500

•  Number of masons trained in US standards and protocols: 200

•  Number of engineers trained in US standards and protocols: 35

•  Foundations: built of reinforced concrete

•  Cell masonry: 

         • Used 2-cell masonry blocks, which are less susceptible to breakage, accept the

           vertical steel elements and additional concrete, and have higher compressive

           strength. 

•  Wall reinforcement:

           • Horizontal and vertical steel in the masonry to take the lateral (horizontal) and gravity

             (vertical) loadings on the wall. 

           • Provides a redundant system where the walls act as hundreds of columns and are

             also reinforced withstand earthquakes and wind.

• Long span roof: 

          • Steel used throughout roof and tied to walls.

          • Creates a “cage” for the entire building and distributes weight more evenly to the

            walls.

          • The slope of the roof allows for drainage and also for ventilation and natural light into

             the classroom


 

ABOUT HONEYWELL
Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

 

Media Contact:
Kelly Reed
(973) 455-2728
Kelly.reed@honeywell.com 

 

  Back to Index Top