Press Releases
  Back to Index
1/24/2012 
Honeywell Launches Full-Scale Smart Grid Project To Reduce Strain On Electrical Networks In The UK 

 

London-Area Pilot Proves Automated Demand Response Can Cut Peak Energy Use in Commercial and Industrial Facilities, Leads to Broad Deployment

 

MINNEAPOLIS, Jan. 24, 2012 — Honeywell (NYSE: HON) today announced a smart grid project that will help SSE plc connect up to 30 commercial and industrial buildings in the Thames Valley area west of London, and temporarily reduce electricity consumption when overall use spikes. This will help alleviate the potential for future transmission and distribution bottlenecks as the peak demand for energy grows. It will also enable building operators to decrease their energy use, utility bills and carbon dioxide emissions.


As part of the £30-million New Thames Valley Vision (NTVV) project recently awarded    to Scottish and Southern Energy Power Distribution (SSEPD) by U.K. energy regulator Ofgem, Honeywell will install automated demand response (Auto DR) technology in the selected facilities. The utility will then work with these customers to trim peak electricity use, and reduce strain on the local networks and substations, which are nearing capacity — creating a more robust, agile grid without the disruption and expense which sometimes accompany major infrastructure upgrades.


“NTVV has the potential to revolutionize our existing networks, and help us to manage resources and equipment more effectively as the U.K. heads toward a low-carbon economy,” said Stewart Reid, NTVV Project Director at SSEPD. “We’ll need to collaborate with our customers to achieve these goals and see Auto DR as a one of the key tools to make that a reality.”


The project builds on a successful Auto DR demonstration in Bracknell, England, where Honeywell proved that a commercial building could quickly shed up to 45 percent of its electrical load during peak hours. The result of the pilot prompted SSE to expand the use of the technology. Honeywell expects the full-scale project will give the utility the ability to shave approximately      10 megawatts of energy use when necessary.  


“A smarter grid is essential to balancing supply and demand in the most efficient, sustainable way possible,” said Paul Orzeske, president of Honeywell Building Solutions. “But utilities also need to connect with their customers in new ways and Auto DR creates those bonds. It’s flexible enough to meet a variety of energy challenges, from daily grid congestion issues to intermittency concerns that stem from micro-generation.”


Honeywell will use several technologies in its portfolio, including offerings from Honeywell’s Akuacom and Tridium businesses, to connect SSE with buildings on the utility’s low-voltage Bracknell network. The Demand Response Automation Server (DRAS) from Akuacom allows the utility to alert customers when energy use is expected to peak and create grid congestion. At each facility, a NiagaraAX Framework-based controller from Tridium will help automate load-shedding strategies during these periods. The controller listens for signals from the DRAS and communicates with the building management system, which then makes short-term changes based on parameters the customer sets in advance — e.g., turning off banks of lights or elevators, or cycling equipment on and off.


In addition to providing and implementing the technology, Honeywell will offer consulting and engineering services to help the customers develop shed strategies, looking for ways to briefly reduce energy use with minimal impact to operations. Honeywell will also investigate opportunities to decrease day-to-day consumption, which will help participants reduce their operating costs and environmental impact, and align with Carbon Reduction Commitment legislation.


As part of the agreement with Ofgem, SSE and Honeywell will also publish details on the project and its impact to provide insight for other distribution network operators (DNOs) across the United Kingdom.

 

Automated Demand Response
Buildings account for more than 70 percent of electricity use globally. Auto DR enables utilities to call on commercial facilities to automatically decrease consumption during times of peak demand, reducing the load on the electrical network. Building operators work with an energy expert like Honeywell to develop custom strategies to decrease their energy use, utility bills and carbon dioxide emissions. DNOs, in turn, are able to alleviate grid congestion caused by growing demand and the pressure it puts on transmission and distribution equipment. The prevailing alternative is to replace or reinforce the sub-stations, electrical cables and associated equipment, which requires significant capital investment and construction in highly developed urban areas. 


Previous demand response programs have been largely manual and cumbersome to initiate; as a result, building operators had to dedicate the necessary resources to participate and utilities couldn’t count on a consistent response. The Akuacom and Tridium technologies are able to interact with virtually any building system, providing a reliable decrease in consumption with minimal input. That’s because the solution is based on open, industry-accepted standards.

 

Honeywell and the Smart Grid
Honeywell has a legacy of working with both utilities and their customers, giving it a unique perspective on how to quickly realize the benefits of the evolving grid. With controls in more than 150 million homes, 10 million buildings and thousands of industrial sites, and experience managing demand response and energy efficiency programs for more than 100 utilities, Honeywell has the offerings and experience to empower smart energy users.

 

Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell Building Solutions is part of the Honeywell Automation and Control Solutions business group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Building Solutions, access www.honeywell.com/buildingsolutions.

 

This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

 

Media Contacts:
Aaron Parker         
Honeywell        
+1 763 954 4257       

aaron.parker@honeywell.com

 

Louisa Kellie 
Honeywell 
+420 242 442 309
louisa.kellie@honeywell.com  

  Back to Index Top