Press Releases
  Back to Index
10/6/2011 
Honeywell Implements First Automated Demand Response Project For Commercial And Industrial Facilities In Europe 

 

Pilot Project Will Help Scottish and Southern Energy Relieve Electrical Congestion and Develop a Smarter, More Dynamic Grid

 

MINNEAPOLIS, Oct. 6, 2011 — Honeywell (NYSE: HON) today announced it has been selected by Scottish and Southern Energy plc (SSE) to conduct the first automated demand response (Auto DR) pilot project for commercial and industrial facilities in Europe. The Auto DR project will give SSE the ability to work with its business customers to temporarily reduce or shift energy use when overall demand spikes, creating transmission and distribution bottlenecks.


While meeting electricity needs is typically not an issue, the amount of power required to satisfy peak demand is quickly rising, pushing network capacity and creating the potential for future outages. The investment required to replace or reinforce the infrastructure is significant, as is the disruption a large public works project can create. This is a growing concern in urban areas across the U.K. and Europe.


SSE will use the pilot to develop a long-term strategy for Auto DR, and the project will provide valuable insight for other distribution network operators (DNOs) across the continent. The initial deployment is being supported by the Low Carbon Network Fund, which was established by Britain’s energy regulator Ofgem to promote the development of energy conservation technologies and implementation of smart grid solutions.


Stewart Reid, future networks and policy manager for Scottish and Southern Energy, which transmits and distributes electricity to nearly 3.5 million businesses, offices and homes: “SSE’s core purpose is to provide the energy people need in a reliable and sustainable way. Automated demand response is one of a portfolio of tools to make sure we do that, and we are pleased to be working with Honeywell on this project in the Thames Valley.”


As part of the pilot, Honeywell will use several technologies in its portfolio — including offerings from Akuacom and Tridium — to connect SSE with commercial and industrial buildings on the utility’s Bracknell network in southern England. The Demand Response Automation Server (DRAS) from Akuacom allows the utility to alert customers when energy use is expected to peak and create grid congestion. At each facility, a Tridium controller will help automate load-shedding strategies during these periods. The controller listens for signals from the DRAS and communicates with the building management system, which then makes short-term changes based on parameters the customer sets in advance. The changes range from turning off banks of lights to cycling equipment on and off.


In addition to providing and implementing the technology, Honeywell will offer consulting and engineering services to help the customers develop shed strategies, looking for ways to briefly reduce energy use with minimal impact to operations. Honeywell will also investigate opportunities to decrease day-to-day consumption, which will help participants reduce their operating costs and environmental impact, and align with Carbon Reduction Commitment legislation.


This is pioneering work by SSE and Honeywell since previous programs have been largely manual and cumbersome to initiate, which meant building operators had to dedicate the necessary resources to participate and utilities couldn’t count on a consistent response. The Akuacom and Tridium technologies are able to interact with virtually any building system, providing a reliable decrease in consumption with minimal input. That’s because the solution is based on open, industry-accepted standards. Should SSE decide to change solution providers, it can do so without the risk and cost of stranded assets.


Paul Orzeske, president of Honeywell Building Solutions: “We were the first to apply Auto DR technology in Asia and North America. And the pilot with SSE will help prove that it’s portable and flexible enough to meet the challenges of utilities around the world. Reducing peak demand and increasing efficiency are some of the greenest and cleanest options when it comes to energy. So we’re excited to demonstrate the benefits to SSE and the broader community, and set the stage for implementations on a much larger scale.”


Honeywell has a legacy of working with both utilities and their customers, giving it a unique perspective on how to quickly realize the benefits of the evolving grid. With controls in more than 150 million homes, 10 million buildings and thousands of industrial sites, and experience managing demand response and energy efficiency programs for more than 100 utilities, Honeywell has the offerings and experience to empower smart energy users.

 

About Auto DR
Buildings account for more than 70 percent of electricity use globally. Auto DR enables utilities to call on commercial facilities to automatically decrease consumption during times of peak demand, reducing the load on the electrical network. Building operators work with an energy expert like Honeywell to develop custom strategies to decrease their energy use, utility bills and carbon dioxide emissions. DNOs, in turn, are able to alleviate grid congestion caused by older transmission and distribution equipment, which is already stressed and struggling to handle the necessary throughput. The prevailing alternative is to replace or reinforce the electrical network and associated equipment, which requires significant capital investment and construction in highly developed urban areas.      


Auto DR is also a key tool in the broad integration of renewable energy, such as wind and solar, because it can help absorb the inherent variability of those resources.

 

Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell Building Solutions is part of the Honeywell Automation and Control Solutions business group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Building Solutions, access www.honeywell.com/buildingsolutions.

 

This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

 

Media Contacts:
Aaron Parker         
Honeywell       
+1 763 954 4257       
aaron.parker@honeywell.com

 

Louisa Kellie
Honeywell
+420 242 442 309
louisa.kellie@honeywell.com

  Back to Index Top