Press Releases
  Back to Index
6/18/2011 
Honeywell Green Jet Fuel™ Powers First-Ever Transatlantic Biofuel Flight 

 

• Use of Honeywell Green Jet Fuel saves 5.5 metric tons of net carbon dioxide emissions
• Green Jet Fuel now one step closer to commercial use with initial ASTM approval
• Honeywell biofuel and aviation technologies drive down flight costs, increasing profits and reducing carbon footprints

 

PARIS, June 18, 2011 – Honeywell (NYSE: HON) announced today that its Green Jet Fuel has successfully powered the first transatlantic biofuel flight, which landed today at Paris-Le Bourget Airport.


The Honeywell-operated Gulfstream G450 became the first aircraft to fly from North America to Europe with a 50/50 blend of Honeywell Green Jet Fuel and petroleum-based jet fuel, powering one of the aircraft’s Rolls-Royce engines. It was also the first business jet to be powered by a biofuel.


The biofuel was derived from camelina, a dedicated energy crop that does not compete in the food chain as it grows in rotation with wheat acreage and can also grow on marginal land. The feedstock for this flight was grown and harvested by Sustainable Oils, a U.S.-based producer of camelina-based technology.


 The flight departed Morristown, N.J., at 9 p.m. Friday and arrived in Paris about seven hours after takeoff. The jet closely followed the route taken by Charles Lindbergh’s famous first flight across the Atlantic. More details about the Honeywell flight and its path can be found here http://inr.stage.synapticdigital.com/HoneywellAerospace/ParisAirShow2011/.


Based on lifecycle analyses, use of Honeywell Green Jet Fuel on the flight saved approximately 5.5 metric tons of net carbon dioxide emissions compared to the same flight powered by petroleum-based fuel.

 
“This first biofuel trip across the Atlantic, along with more than a dozen other commercial and military test flights conducted to date, demonstrates that Honeywell Green Jet Fuel more than meets the demanding requirements for air travel,” said Jim Rekoske, vice president and general manager of Renewable Energy and Chemicals for Honeywell’s UOP. “Now that the initial ASTM International approval is in place, we are one step closer to commercial use that will help the aviation community reduce its carbon footprint and dependence on crude.”


"Gulfstream is committed to achieving business aviation's ambitious goals on emissions reductions," said Pres Henne, senior vice president, Programs, Engineering and Test for Gulfstream. "These include carbon neutral growth by 2020 and a reduction in total carbon emissions of 50 percent by 2050 relative to 2005. We are working with engine companies and other innovators, such as Honeywell, to ensure we can meet these initiatives. We are very proud to participate in this historic demonstration."

 

Advancing New Sources of Fuel to Reduce Aviation Emissions


Fluctuating fuel prices combined with increased restrictions in aviation emissions regulations drive the demand for alternative sources of fuel. Honeywell Green Jet Fuel is a sustainable fuel option that meets all specifications for flight without any modifications to the aircraft or engine.


Honeywell has produced more than 700,000 gallons of Honeywell Green Jet Fuel from sustainable, inedible sources such as camelina, jatropha and algae for use in commercial and military testing. In each of the 16 biofuel flights conducted to date, Honeywell Green Jet Fuel proved that it meets all specifications for flight on military and commercial platforms without any modification to the aircraft or engines.


The process to produce Green Jet Fuel was originally developed in 2007 under a contract from the U.S. Defense Advanced Research Projects Agency (DARPA) to produce renewable military jet fuel. The process is based on hydro-processing technology commonly used in today’s refineries to produce transportation fuels. It produces an aviation biofuel that can be blended seamlessly with petroleum-based fuel.


“With more than 500,000 gallons produced, camelina-based renewable jet fuel has been the most widely tested of any feedstock and has proven itself on more engine types and aircraft,” said Tom Todaro, CEO of Sustainable Oils. “It’s the only sustainable feedstock that is widely and commercially available today. We are proud to partner with Honeywell on this historic flight.”

 

Driving Down Airlines’ and Operators’ Cost of Operations and Reducing Carbon Footprint
In addition to biofuels, Honeywell offers a range of technologies to help airlines reduce fuel costs -- the largest single operating cost for airlines.


“Reducing both the cost of operations and carbon emissions has never been more imperative. From advanced avionics to sustainable biofuel and energy efficient jet engines, innovations from Honeywell are addressing these needs today,” said Carl Esposito, vice president of strategy and product management for Honeywell Aerospace. “Honeywell’s PRIMUS EPIC navigation and safety technologies embedded in Gulfstream’s PlaneView cockpit helped the aircraft fly the most fuel efficient and direct route from Morristown.”


Honeywell technologies also support worldwide air traffic modernization efforts to make flights safer, more fuel efficient, and can lower emissions. Honeywell’s Air Traffic Management technologies and Flight Management Systems (FMS) also help to shorten flight times, increase flight efficiency and safety through precision navigation and landing systems; and minimize airport delays and carbon footprint.


 Honeywell’s newly certified advanced traffic collision avoidance system (TCAS) solution with SmartTraffic can significantly reduce cost of operations for airlines. SmartTraffic incorporates In Trail Procedure (ITP), designed to allow planes to fly closer together and land more efficiently without sacrificing safety. The ability to simply change routes can enable fuel savings of up to $100,000 per year, per aircraft.


Honeywell is also helping to develop the next generation air traffic management system that uses GPS satellites rather than radar.


Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

 

Honeywell and the Honeywell logo are the exclusive properties of Honeywell International, Inc., are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2011 Honeywell.


This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.

 

Media Contacts:
Susan Gross       
Honeywell UOP      
847-391-2380       
Susan.Gross@honeywell.com      
        
Bill Reavis
Honeywell Aerospace
602-365-2055
Bill.Reavis@honeywell.com
Honeywell Aerospace Media Center 

  Back to Index Top