Improved thermal material significantly decreases use of lead in
semiconductor- power/discrete devices, helping to meet growing demand for more
environmentally friendly solutions
MORRIS TOWNSHIP, N.J., March 16, 2009 -- Honeywell (NYSE: HON) announced
today that it has developed a new lead-free packaging technology that improves
the thermal management of semiconductor chips.
The new product, called Honeywell Pb-free Die Attach Solder, is a lead-free
thermal interface material that effectively manages the tremendous heat
produced by semiconductor chips in order to improve chip reliability.
“Honeywell has been developing lead-free die attach solder alloys for many
years to meet the industry’s ‘green’ requirements that emerged with the use of
lead-free solder at the circuit board level,” said Scott Miller, metals product
line manager for Honeywell Electronic Materials. “Our newest alloys will
replace the high-lead alloys and provide better thermal management than other
proposed lead-free thermal management alternatives such as polymer-based
materials.”
As semiconductors become more powerful and smaller, more heat is being
generated in a confined space when semiconductors are packaged for use in
computers and other applications. This tremendous heat can damage the
semiconductor or degrade its performance. Honeywell’s thermal management
materials are designed to help the semiconductor packaging industry dissipate
this heat by filling the gap between the semiconductor and the heat
spreader.
Demand for lead-free solders is growing, driven in part by regulation.
Honeywell’s new Pb-free Die Attach Solder is an advanced technology that is not
only better for the environment, but is also cost effective. Lead-based solders
are currently used for power/discrete die attach because they have a very good
combination of melting temperature, wetting behavior, and mechanical
properties. The new lead-free solder alloys are designed to meet these
requirements, particularly resistance to melting during board level solder
reflow.
Targeting the semiconductor industry’s power device segment, Pb-free Die Attach
Solder will be used in chips that service a wide range of industries, from
automotives to cell phones.
The lead free material is based on Honeywell’s metallurgical expertise and long
experience as a supplier of die-attach solders. Honeywell Pb-free Die Attach
Solder is designed to be used mainly in wire form and compliments Honeywell’s
large diameter aluminum wire products. It provides power device manufacturers
with a lower cost, more effective and greener alternative.
Honeywell Electronic Materials, part of Honeywell Specialty Materials, supplies
microelectronic polymers, electronic chemicals, and other advanced materials
that enable the integration of cutting edge processes at customer sites.
Honeywell also maintains extensive product offerings under its metals business
segment, including physical vapor deposition (PVD) targets and coil sets,
precious metal thermocouples and materials used during back-end packaging
processes for thermal management and electrical interconnect. More information
can be found at http://www.honeywell.com/em/.
Honeywell International is a $37 billion diversified technology and
manufacturing leader, serving customers worldwide with aerospace products and
services; control technologies for buildings, homes and industry; automotive
products; turbochargers; and specialty materials. Based in Morris Township,
N.J., Honeywell’s shares are traded on the New York, London and Chicago Stock
Exchanges. For additional information, please visit www.honeywell.com.
This report contains “forward-looking statements” within the meaning of Section
21E of the Securities Exchange Act of 1934. All statements, other than
statements of fact, that address activities, events or developments that we or
our management intend, expect, project, believe or anticipate will or may occur
in the future are forward-looking statements. Forward-looking statements are
based on management’s assumptions and assessments in light of past experience
and trends, current conditions, expected future developments and other relevant
factors. They are not guarantees of future performance, and actual results,
developments and business decisions may differ from those envisaged by our
forward-looking statements. Our forward-looking statements are also subject to
risks and uncertainties, which can affect our performance in both the near- and
long-term. We identify the principal risks and uncertainties that affect our
performance in our Form 10-K and other filings with the Securities and Exchange
Commission.
Contacts:
Peter Dalpe
973-455-4908
Peter.Dalpe@honeywell.com
Alexandra Pribilovics
+86 (21) 2894-2932
Alexandra.Pribilovics@honeywell.com