Press Releases
  Back to Index
2/21/2010 
Honeywell Announces HTS900 Engine Upgrade For Bell 407 Operators 

New Upgrade Delivers 40 Percent More Payload at Altitude

HELI-EXPO®, Houston, Feb. 21, 2010 -- Honeywell (NYSE: HON) announced today that it has teamed with Eagle Copters of Calgary, Alberta, to offer an HTS900 engine upgrade for the Bell 407 helicopter, called the Eagle 407 HP.

“Eagle 407 HP operators are going to see a big difference, especially flying cargo high or hot, because of a 26 percent increase in shaft horsepower,” said Carl Esposito, vice president, Marketing & Product Management, Honeywell Aerospace. “The HTS900 fills the Bell transmission with power up to 14,500 feet.”

The new Eagle 407 HP, using design and engineering licensed from Bell Helicopter, will provide operators up to a 40 percent increase in Hover-Out-of-Ground-Effect (HOGE) performance at International Standard Atmosphere (ISA) +20°C conditions, while delivering a 10 percent reduction in fuel consumption. The increased altitude payload allows for full onboard mission equipment and fuel capacity, allowing mission completion without repeat flights.

“The Eagle 407 HP transforms the Bell 407 into a real high-hot performer,” said Mike O’Reilly, president of Eagle Copters. “Using Bell Helicopter design and engineering adds an enormous credibility to the design.”

The Honeywell HTS900 engine is a new type of engine design that provides superior performance in high, hot conditions, fuel efficiency and operating costs. New technologies include a dual centrifugal compressor, cooled single-crystal turbine blades, effusion cooled combustor liner, and a dual-channel Full Authority Digital Engine Control (FADEC).

“The HTS900 engine delivers more than 1,000 Shaft Horsepower (SHP) and the lowest fuel consumption and highest power-to-weight ratio of any engine in its class,” said Esposito. “The HTS900 upgrade delivers 10 percent lower fuel burn and on-condition maintenance with no hard time overhaul limits, achieving a 10 percent lower operating cost.”

Honeywell offers a full range of helicopter equipment, from aircraft engines, auxiliary power units and other mechanical systems to the Zing™ Health Usage Monitoring Systems (HUMS). Honeywell's safety systems for helicopters address the challenges of traffic, terrain and weather, helping to ensure safe flight and guard against Controlled Flight Into Terrain (CFIT), weather related hazards, and collisions with obstacles and other aircraft.

Based in Phoenix, Arizona, Honeywell’s aerospace business is a leading global provider of integrated avionics, engines, systems and service solutions for aircraft manufacturers, airlines, business and general aviation, military, space and airport operations.

Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.

Media Contacts:
Carrie Sinclair
602-365-2324
Carrie.Sinclair@honeywell.com
twitter.com/HON_Carrie

Bill Reavis
602-365-2055
Bill.Reavis@honeywell.com
Honeywell Aerospace Media Center


  Back to Index Top  
 

Media Relations Contact