Press Releases
  Back to Index  
Text Size:  
World’s Leading Automotive Engineering Organization And Eleven Global Automakers Conclude That Honeywell’s Low-Global-Warming Refrigerant Is Safe For Use In Automobiles 


SAE International Cooperative Research Project’s expanded, extensive evaluation of HFO-1234yf refrigerant shows no change in its previous safety conclusions; Reiterates that concerns raised by one automaker based on “unrealistic” testing

MORRIS TOWNSHIP, N.J., June 25, 2013 – Honeywell (NYSE: HON) announced today that SAE International, the world’s leading automotive engineering association, has concluded that Honeywell’s new low-global-warming-potential mobile air conditioning refrigerant, HFO-1234yf, is safe for use in automobiles after completing an expanded and extensive evaluation.

The SAE International Cooperative Research Project (CRP) also said that all 11 global automakers who participated in the project “have indicated agreement with these conclusions” and called testing conducted by Daimler late last year that raised questions about the refrigerant’s flammability “unrealistic.”

“After extensive testing and analysis, the new CRP concluded that the refrigerant release testing completed by Daimler was unrealistic,” the SAE CRP said in its final summary. “Their testing created extreme conditions that favored ignition while ignoring many mitigating factors that would be present in an actual real-world collision.”

“The conclusions from SAE’s latest expanded evaluation, combined with years of extensive testing in the U.S., Europe and elsewhere, again leaves no doubt that HFO-1234yf is safe for automotive applications,” said Ken Gayer, vice president and general manager for Honeywell Fluorine Products. “The fact that all 11 global automakers participating in the project agreed with the SAE CRP’s conclusions is further proof that this product can be used safely.”

The latest CRP included European, North American, and Asian automakers, including Chrysler/Fiat, Ford, General Motors, Honda, Hyundai, Jaguar Land Rover, Mazda, PSA, Renault and Toyota.

HFO-1234yf, a highly-efficient, safe and effective replacement for HFC-134a, is already in use by the auto industry. It is being adopted by automakers in part to meet the European Union’s Mobile Air Conditioning (MAC) Directive, which aims to reduce the greenhouse gas emissions of air-conditioning systems in passenger cars and light commercial vehicles. The directive requires that refrigerants in all new type vehicles sold in Europe after Jan. 1, 2013, have a global-warming potential (GWP) below 150 and that all cars sold after 2017 meet the lower GWP requirement.

HFO-1234yf has a GWP of 4 and reduces global warming impact by 99.7 percent compared with HFC-134a. According to third-party data, HFO-1234yf’s adoption in cars today would have the greenhouse gas equivalent impact of removing more than 4 million cars from European roads.

HFO-1234yf was the subject of comprehensive testing conducted by an SAE CRP from 2007 to 2009. That CRP, which was sponsored by 15 global automakers, including all leading German automakers, major suppliers and 18 international, independent research institutes, concluded that HFO-1234yf is safe for use in automobile applications.

SAE initiated the latest CRP after Daimler raised questions about the refrigerant’s flammability. SAE said its latest CRP’s evaluation was expanded “with input from Daimler … to realistically address” Daimler’s concerns. SAE said the CRP also reviewed and analyzed extensive new data from automakers and used “conservative assumptions” to ensure its analysis “would be more likely to overestimate rather than underestimate the actual risks” of the refrigerant igniting.

Even with those assumptions, the CRP found “risks are still very small compared to the risks of a vehicle fire from all causes and well below risks that are commonly viewed as acceptable by the general public.”

The SAE concluded it was 20,000 times more likely for a person to die in a plane crash than be exposed to a vehicle fire caused by a leak and ignition of HFO-1234yf. It also said it was 300,000 times more likely a vehicle would experience a fire for any reason and 100,000 times more likely for an accident to happen because of a brake failure.

The CRP has said throughout its evaluation that it used universally accepted engineering methods, including analysis of recent OEM testing from actual vehicle crash data, on-vehicle simulations, laboratory simulations, bench tests, and over 100 engine compartment refrigerant releases. It also employed fault-tree analyses, which it noted have been recommended and employed by numerous public and private organizations, including the U.S. Environmental Protection Agency, the U.S. Department of Energy, the International Electrotechnical Commission, the European Union Joint Research Centre, and the United Kingdom Health and Safety Executive.

SAE International, formerly known as the Society of Automotive Engineers, is an independent, global association of more than 133,000 engineers and related technical experts in the aerospace, automotive and commercial-vehicle industries.

Under rare conditions, HFO-1234yf exhibits mild flammability, at levels significantly lower than highly flammable materials already present under the hood of an automobile, including motor oil, automotive transmission fluid, radiator antifreeze, brake fluid, and compressor lubricant – not to mention fuel. For a video on this topic, which includes a comparison of HFO-1234yf vs. HFC-134a and other materials, visit or

Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit

This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

Peter Dalpe
(973) 455-4908

  Back to Index Top