Press Releases
  Back to Index  
Text Size:  
6/17/2014 
Honeywell Marks Centennial Of Aerospace, Oil And Gas Leadership 

 

Honeywell Aerospace and UOP continue legacy of innovation

 

NEW YORK, June 17, 2014 Honeywell (NYSE: HON) marked 100 years of innovation and leadership in the aerospace and oil and gas industries as Honeywell Chairman and CEO Dave Cote led other company executives in ringing the closing bell at the New York Stock Exchange. The bell ringing recognized the centennials of Honeywell Aerospace, a pioneer in aviation, and Honeywell’s UOP, which created the basis for the modern refining industry.

 

Honeywell Aerospace traces its legacy of innovation to June 18, 1914, when Lawrence Sperry did a “wing walk” with no one at the controls of his airplane to demonstrate the first aircraft stabilizer, which became known as the autopilot. Today, Honeywell has one of the largest aerospace products and services portfolios in the industry, having invented hundreds of technologies that have led to safer skies, space exploration and stronger military offerings. Honeywell offers thousands of products and services that can be found on virtually every commercial, defense and space aircraft worldwide.

 

UOP was founded in Chicago on June 17, 1914, to commercialize the first conversion technology for upgrading crude oil, resulting in a fourfold increase in the amount of gasoline that could be derived from crude oil. Now part of Honeywell’s Performance Materials and Technologies (PMT) business, UOP remains the recognized leader for providing process technology, catalysts, adsorbents, equipment and consulting services to the petroleum refining, petrochemical and gas processing industries.

 

Continuous Advancements in Oil and Gas Technology

UOP became a wholly owned subsidiary of Honeywell in 2005. Since then, UOP’s revenue has more than doubled as Honeywell has invested in its growth.

 

 “UOP has been and continues to be a driving force of innovation for the global petroleum and natural gas industries,” said Rajeev Gautam, president and CEO of UOP. “Our partnership with the world’s oil and gas companies has led to the development and commercialization of the technologies that have enabled our modern way of living.”

 

During the past 100 years, UOP breakthroughs include technologies to more efficiently produce gasoline, diesel fuel and jet fuel, and to manufacture the chemical compounds that helped launch the modern petrochemicals industry, introducing the world to products made from plastic resins and films and synthetic fibers. UOP commercialized technologies to produce the first large-scale biodegradable detergents, produce lead-free gasoline and make possible the automobile catalytic converter. The world’s leading developer of technologies for the oil and gas industry, UOP has earned more than 12,000 patents.

 

UOP’s innovations continue today with process technologies to get more valuable products from every barrel of oil, to convert coal and natural gas into plastics, and to convert biofeedstocks such as algae into renewable fuels. The company also develops technologies to grow the availability of natural gas and treat it so it can be shipped around the world.

In 2003, UOP was recognized by President George W. Bush with the National Medal of Technology and Innovation for “sustained technical leadership and innovation for the petroleum refining and petrochemical industries; and for the invention and commercialization of adsorbents, catalysts, process plants, and process technology.”

 

Honeywell Aerospace Firsts

For more than a century, Honeywell Aerospace has helped write aviation history, with a major focus on flight safety. “I’m proud to be part of a company that has accomplished so much including the invention of the autopilot 100 years ago. We are just getting started, and we will continue to provide innovative aviation solutions that make the possibilities of flight even safer, more efficient, more comfortable, more productive and higher performing,” said Tim Mahoney, president and CEO, Honeywell Aerospace. “With the rapid pace of technology evolution such as our work on wireless connectivity, Honeywell will be at the forefront of incredible aviation innovation in the coming decades that outshines the amazing things we’ve done this past century.”

 

 Together with its legacy companies and in addition to the first autopilot, other Honeywell Aerospace inventions include:

  • The first gyro horizon and directional gyro, invented in the 1920s, proved the practicality of instrument-only flight with advanced navigation.
  • In the 1940s, technology inventions led to the advent of cabin pressurization, which enabled higher-flying aircraft and space exploration.
  • The first gas turbine Auxiliary Power Unit (APU), invented in 1948, revolutionized commercial air travel to remote regions when it was first installed on the Boeing 727 in the 1960s, providing independent startup and backup power. The APU played a critical role in the emergency landing of US Airways Flight 1549 in New York’s Hudson River, ensuring the safety of 155 passengers onboard.
  • The first Ground Proximity Warning System (GPWS) was invented in the 1970s and the Enhanced GPWS (EGPWS) in the 1990s have helped pilots avoid flying into unseen mountains and other terrain. The technologies have been credited with saving thousands of lives.
  • The first complete 3-D picture of airborne weather conditions, Honeywell’s IntuVue weather radar, was developed in 2008. The technology helps increase in-flight pilot awareness and safety, while enhancing passenger comfort, by avoiding poor weather conditions and turbulence.

 

Honeywell Aerospace continues to invest in research and technology and is committed to bringing to the industry the latest solutions in safety, connectivity, energy efficiency, air traffic management and more.

 

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

 

Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2014 Honeywell.

 

Media Contacts:

Gwennie Cheung
Honeywell Aerospace
(646) 589-1741
Gwennie.Cheung@Honeywell.com
Honeywell Aerospace Newsroom
 

John Simley
UOP

(847) 391-2278
John.Simley@Honeywell.com
UOP Newsroom

  Back to Index Top