Press Releases
  Back to Index  
Text Size:  
Honeywell’s UOP Launches New Membrane Element To Improve Contaminant Removal From Natural Gas 


New UOP SeparexTM Select membrane element improves contaminant removal, meaning less loss of valuable methane and natural gas liquids

DES PLAINES, Ill., March 12, 2013 -- UOP LLC, a Honeywell (NYSE: HON) company, today announced the launch of a new membrane element that more efficiently removes contaminants from natural gas and reduces the amount of valuable methane and natural gas liquids (NGLs) lost during the contaminant removal process.

Honeywell’s UOP Separex™ Select membrane element is the next-generation technology to remove contaminants such as acid gas and water from natural gas. Methane, or dry natural gas, is in high demand for heating and power generation, while NGLs are valuable feedstock for the production of petrochemicals such as plastics.

“UOP is dedicated to introducing more efficient gas processing technologies that help maximize the recovery of valuable methane and natural gas,” said Rebecca Liebert, vice president and general manager of Honeywell’s UOP Gas Processing and Hydrogen business unit. “With the addition of Separex Select, UOP now offers the broadest portfolio of advanced membrane elements, designed to enable gas producers to tailor solutions for highest value, minimal cost and operational ease.”

Separex Select membrane elements are designed as a replacement option for the elements currently housed within Honeywell’s UOP Separex systems. These elements upgrade natural gas streams by removing carbon dioxide, hydrogen sulfide and water vapor in a single process to meet the quality standards specified by pipeline transmission companies and end-users of the natural gas.

Honeywell’s UOP developed Separex Select as a more selective element in gas separation. It offers an increase in membrane selectivity compared with existing cellulose acetate (CA) membrane elements, driving significantly higher recovery of methane and NGLs, while simultaneously reducing hydrocarbon emissions. In multi-stage Separex systems, Separex Select can also help producers lower their operating costs due to reduced inter-stage compression requirements.

Honeywell’s UOP is continuously working to improve and expand its Separex membrane portfolio, along with all of its natural gas processing technologies. Earlier this year, it announced the launch of Separex Flux+ membrane elements. These drop-in replacements for Separex membrane systems allow higher processing capacity compared with the industry standard. Honeywell’s UOP also offers Separex Flux, a CA membrane with optimized capacity and selectivity, which has been the cornerstone of the Separex membrane system during the last 30 years.

Decades of operation in natural gas service have demonstrated that Honeywell’s UOP Separex membranes are the most robust for natural gas contaminant removal and can achieve the longest membrane life in the industry. Separex membranes eliminate the need for solvents, making the technology particularly desirable in remote locations where logistics make supply transportation to the site difficult. Because Separex membrane elements are inert solids, these membranes offer a spill-free, ecosystem-friendly solution. Separex membrane systems can be installed on-shore or off-shore, require little to no utilities, and provide for very short start-up times and high turndown capabilities. To date, more than 130 Separex units have been installed worldwide.
Honeywell’s UOP Gas Processing and Hydrogen business offers technology, equipment and materials to treat and process natural gas, as well as to purify hydrogen used in refineries. Its gas technologies extract contaminants such as water, mercury, sulfur and carbon dioxide from raw natural gas. Honeywell’s UOP also offers technologies to recover NGLs. The business has supplied technology to more than 3,600 individual process units for gas processing in a broad range of applications through the world, including Floating, Processing, Storage and Offloading (FPSO) vessels.

Honeywell’s UOP has increased its offerings in natural gas in recent years. In 2012, the company purchased a majority stake in Thomas Russell Co., which offers key technologies and modularized packaged plants enabling shale and conventional natural gas producers to remove contaminants from natural gas and recover high-value NGLs used for petrochemicals and fuels. Thomas Russell products are now part of the UOP Russell line. Honeywell’s UOP also has marketing alliances with Twister B.V., and Ortloff Engineers Ltd. for natural gas separation technology to recover NGLs.

Honeywell’s UOP Gas Processing and Hydrogen business has also expanded its global footprint, opening a gas processing design center in Kuala Lumpur, Malaysia, in 2008. In 2011, it opened a manufacturing and operations center to produce natural gas membrane elements in Penang, Malaysia, to better serve growing natural gas markets in Southeast Asia and around the world.

UOP LLC, headquartered in Des Plaines, Illinois, USA, is a leading international supplier and licensor of process technology, catalysts, adsorbents, process plants, and consulting services to the petroleum refining, petrochemical, and gas processing industries. UOP is a wholly-owned subsidiary of Honeywell International Inc. and is part of Honeywell’s Performance Materials and Technologies strategic business group. For more information, go to

Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit

This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.


Krystal Hughes
(847) 391-3561

  Back to Index Top