- Press & Media
- Honeywell’s Healthy Buildings Experts Recommend Strategies to Improve Indoor Air Quality in Reopened Schools
Honeywell’s Healthy Buildings Experts Recommend Strategies to Improve Indoor Air Quality in Reopened Schools
Limiting exposure and spread of virus indoors requires a ‘layered’ approach that includes air quality monitoring, ventilation, air cleaning and occupancy analytics
October 1, 2021
ATLANTA, October 1, 2021 -- With schools around the country back in session, school administrators are assessing methods and technologies to improve indoor air quality (IAQ) and reduce potential exposure to airborne contaminants. A recent survey conducted by Honeywell (Nasdaq: HON) found that 77% of surveyed U.S. facility managers in the education sector say COVID-19 has caused them to permanently rethink how their facility operates, and 34% said they are planning to invest in IAQ solutions in the next 12 to 18 months.[i]
“The demand for better indoor air quality isn’t just about responding to COVID-19. As science increasingly points to the correlation between healthier indoor air and well-being, we expect to see improved air quality on the ‘must have’ list of parents and educators,” said Manish Sharma, vice president and chief technology and product officer of Honeywell Building Technologies. “By taking advantage of federal funding and following expert guidelines, schools have an opportunity to invest in better air and ultimately in the improved performance and well-being of students, teachers and their communities.”
Honeywell Healthy Building engineers recommend that school administrators take immediate action to assess and address the state of school environments, including the following steps:
Install sensors to actively monitor factors that impact IAQ.
IAQ can be impacted by a number of different factors, including: particulate matter, volatile organic compounds (VOC), CO2, temperature and humidity. IAQ sensors monitor these factors and help inform necessary adjustments to meet recommended parameters. Ideal indoor relative humidity should range from 40 to 60%[ii] to help reduce the spread of airborne pathogens. Simultaneously, indoor air temperature should range between 68.5 to 80.5 degrees F[iii], depending on the season (cooler in the winter, warmer in the summer).
“We’re seeing people focus on just one factor – CO2 – as the proxy measurement for indoor air quality,” said Sharma. “While CO2 is important, school facility managers should be actively monitoring a range of parameters, such as particulate matter, VOCs, temperature, humidity, and air pressure, to name a few, and take appropriate automated actions related to filtration, ventilation and pressurization to create healthier indoor air.”
Place portable HEPA air purifiers in high traffic areas to reduce distribution of airborne contaminants and pull contaminated air away from occupants.
Mobile air purifiers with HEPA filters and activated carbon filters are known to capture particles as small as 0.3 microns,[iv] offering an effective and cost-conscious option for schools. Moreover, plug-and-play solutions like portable air purifiers do not require infrastructural changes as they operate independently of HVAC systems. They can be particularly useful in buildings that don’t have forced-air heating or ventilation.
A recent study by Honeywell used computer modeling to simulate air flow and movement of particulates, such as dust, dirt, smoke and respiratory droplets, in common areas of hotels. In the study, 97% of small particles were captured by air purifiers, which made a significant impact on the improvement of air quality.[v]
Maximize ventilation to bring in the maximum amount of outside air when rooms are occupied.
Recent research from the Centers for Disease Control and Prevention found the incidence of COVID-19 was 35% lower in schools[vi] that improved ventilation by opening windows or doors or using fans – and even lower using those tactics in combination with air filtration methods.
Building managers can adjust ventilation in schools and other buildings by extending the operating times of HVAC systems to run before the earliest staff arrive for the day and after the last occupants have left for the night, helping purge air from the building. Fresh air intake should be expanded through natural or mechanical ventilation to the maximum amount possible.
“We cannot mistake just opening windows as effective ventilation. Cracking a window has been the solution some schools have come up with to improve air flow in classrooms but it is not sufficient,” said Sharma. “Ventilation is imperative to improving indoor air quality, but so is effective air filtration, proper pressurization and meeting optimal temperature and humidity levels.”
If energy use is a concern, augment the spaces with filtration solutions like mobile HEPA Air Purifiers to reduce the dependence on ventilation for dilution.
Use analytics to monitor occupancy of rooms and common areas and dynamically adjust indoor air quality parameters.
Schools often have fluctuating occupancy levels in classrooms and common areas. While occupancy can impact indoor air quality, making indoor air quality upgrades isn't something that should wait until occupancy numbers are known. Video analytics and sensors can help schools to track and manage occupancy and adjust indoor air quality parameters dynamically based on how many actual people are in a space.
Advanced video analytics technology allows facility managers to manage compliance to social distancing and face covering guidelines, especially in common areas. The Honeywell Sine mobile solution helps to manage varying occupancy levels, can pre-screen students, staff and visitors with health questionnaires before arrival, and track the flow of people throughout the space when integrated with access management platforms.
About Honeywell Building Technologies
Honeywell Building Technologies (HBT) is transforming the way every building operates to help improve the quality of life. We are a leading building controls company with operations in more than 75 countries supported by a global channel partner network. Commercial building owners and operators use our hardware, software and analytics to help create safe, efficient and productive facilities. Our solutions and services are used in more than 10 million buildings worldwide.
Honeywell (www.honeywell.com/us/en) is a Fortune 100 technology company that delivers industry specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/us/en/news.
[i] Honeywell Building Technologies, Honeywell Survey: Security and Safety Top the List of Education Facility Priorities, July 2021 [Accessed September 8, 2021]
[ii] Honeywell Building Technologies, Know when to clean the air, 2021 [Accessed September 8, 2021]
[iii] CDC, Indoor Environmental Quality, NIOSH, September 2015 [Accessed September 8, 2021]
[iv] EPA, What is a HEPA filter?, March 2021 [Accessed September 8, 2021]
[v] Honeywell, Honeywell Hotel Study Suggests Air Purifiers Help Reduce Exposure to Airborne Contaminants, May 2021 [Accessed September 8, 2021]
[vi] CDC, Mask Use and Ventilation Improvements to Reduce COVID-19 Incidence in Elementary Schools - Georgia, November 16-December 11, 2021, Jenna Gettings, May 2021 [Accessed September 8, 2021]
Copyright © 2024 Honeywell International Inc.