Honeywell technology will enhance safety, increase mission readiness and reduce
maintenance costs for the U.S. Coast Guard
PHOENIX, Dec. 17, 2012 – Honeywell (NYSE: HON) has been awarded a $4.8 million contract to install health and usage monitoring systems (HUMS) onboard the entire fleet of U.S. Coast Guard MH-60T helicopters.
For the U.S. Coast Guard, the installation and use of HUMS is critically important and paramount to the success of its missions. Unscheduled maintenance events can cause mission aborts that are unacceptable in the life-or-death situations that the MH-60T is often called to support. The installation of Honeywell’s Zing® HUMS 1239 greatly increases the U.S. Coast Guard’s ability to complete its mission and has the added benefit of helping reduce maintenance costs.
HUMS is a sensor-based monitoring system that enables preventative maintenance by measuring the health and performance of mission-critical components. By continuously monitoring vibration at numerous points throughout the drivetrain and pinpointing mechanical faults before they become catastrophic failures, HUMS provides actionable information that allows the Coast Guard to anticipate mechanical failures and make anticipatory maintenance decisions. Honeywell’s HUMS products can be installed onboard or used as a portable system for rotor or fixed-wing platforms.
The Coast Guard will use 42 Zing HUMS 1239 aircraft kits and 24 ground support kits, all of which will be delivered before the end of 2012, to monitor critical drivetrain components such as the helicopters’ rotor shafts, making sure that the aircraft is ready to fly at all times. The data collected by the system is easily downloadable into a user-friendly ground station that allows operators to quickly see the status of all selected components instantly, without the costs associated with traditional contractor support.
The U.S. military as well as ministries of defense worldwide use Honeywell HUMS products onboard rotor and fixed-wing aircraft. Honeywell HUMS products are currently installed or in use on the following:
• U.S. Army AH-64D, OH-58D and CH-47D
• All U.S. Army Special Operations Aviation Command rotor wing platforms
• Thousands of commercial rotorcraft including a wide variety of AugustaWestland, Bell Helicopter, Eurocopter, MD Helicopters, Sikorsky and other platforms
Brian Sill, vice president of Defense Americas Aftermarket, Defense & Space, Honeywell Aerospace
• “Honeywell is a leading provider of HUMS solutions for rotor and fixed-wing aircraft around the world. U.S. Coast Guard MH-60T operators will now have key insight and information about potential mechanical issues before they happen, which will help them keep the MH-60T platform running and available when needed.”
Supporting Resources
• Read more about Honeywell Aerospace
• Follow@Honeywell_Aero on Twitter
• Subscribe to Honeywell’s Corporate RSS feed
Based in Phoenix, Arizona, Honeywell’s aerospace business is a leading global provider of integrated avionics, engines, systems and service solutions for aircraft manufacturers, airlines, business and general aviation, military, space and airport operations.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2012 Honeywell.
This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.
Media Contacts:
Nathan Drevna
Honeywell Aerospace
(202) 662-2672
nathan.drevna@honeywell.com
Honeywell Aerospace Media Center
Aaron Grabein
Waggener Edstrom Worldwide
(512) 527-7022
agrabein@waggeneredstrom.com