Antipinsky Refinery will use Honeywell’s UOP Polybed™ PSA System to increase crude oil processing by as much as 7 million tons per year
DES PLAINES, Ill., June 5, 2012 -- UOP LLC, a Honeywell (NYSE: HON) company, announced today that it has been selected by Haldor Topsoe to provide technology to purify hydrogen from a steam reforming unit to be installed at the Antipinsky Refinery in Tyumen, Russia.
UOP’s Polybed™ PSA (Pressure Swing Adsorption) System will recover and purify hydrogen to help the refinery meet the increasing need to produce clean transportation fuels such as diesel and gasoline.
“UOP’s hydrogen purification technology will allow the Antipinksy Refinery to meet today’s challenge of producing cleaner fuels more efficiently,” said Rebecca Liebert, vice president and general manager for gas processing and hydrogen at Honeywell’s UOP. “The impressive hydrogen recovery rates and proven reliability of our solution will help the refinery improve its profitability and ensure dependable operation.”
The new hydrogen unit, which is scheduled to start operating in 2013, is part of the refinery’s plan to increase its capacity of crude oil processing by as much as 7 million tons per year. It will also enable the production of fuel products that meet the European Union’s Euro-5 emission standards aimed at reducing emissions from light duty vehicles.
Refineries use hydrogen in the hydrocracking process to convert heavy oils to lighter, higher-value products such as transportation fuels. Hydrogen is also used in the hydrotreating process to remove contaminants and improve the quality of end products.
To date, Honeywell’s UOP has provided more than 900 Polybed PSA Systems worldwide, including more than 390 units to purify hydrogen from steam reformers, such as at the Antipinsky Refinery. UOP has provided Polybed™ PSA Systems for many Haldor Topsoe hydrogen plants around the world.
The Polybed PSA System is a skid-mounted, modular unit that comes complete with vessels, valve skid, adsorbents, control systems and embedded process technology. The process uses proprietary Honeywell UOP adsorbents to adsorb impurities at high pressure from hydrogen-containing waste streams and subsequently reject them at low pressure. The system allows hydrogen to be recovered and upgraded to more than 99.9 percent purity to meet downstream processing requirements.
In addition to recovering and purifying hydrogen from steam reformers, Polybed PSA Systems can be used to produce hydrogen from other sources, including refinery off-gases, ethylene off-gas, methanol off-gas and partial oxidation/syngas.
Haldor Topsoe is a global supplier of catalysts and technologies, headquartered in Lyngby, Denmark.
UOP LLC, headquartered in Des Plaines, Illinois, USA, is a leading international supplier and licensor of process technology, catalysts, adsorbents, process plants, and consulting services to the petroleum refining, petrochemical, and gas processing industries. UOP is a wholly-owned subsidiary of Honeywell International, Inc. and is part of Honeywell’s Performance Materials and Technologies strategic business group. For more information, go to www.uop.com.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
Media Contact:
Krystal Hughes
(847) 391-3561
krystal.hughes@honeywell.com