Press Releases
  Back to Index  
Text Size:  
Honeywell Survey Explores What Passengers Demand From In Flight Wi-Fi: Constant Connectivity and Speed 



  • In-flight Wi-Fi availability influences flight selection for 66 percent of passengers
  • Nearly one in four admitted they’ve paid more for a flight with Wi-Fi
  • Almost half the respondents would be willing to give up another convenience for Wi-Fi that’s as fast as it is at home, such as enduring airport security twice

PHOENIX, July 22, 2014 – In its second annual survey, Honeywell Aerospace (NYSE: HON) finds that in-flight Wi-Fi is becoming increasingly influential on a passenger’s buying and wireless usage behavior, including flight selections and, in some cases, paying more for a specific flight.


Following up on the 2013 Wireless Connectivity survey, and as the popularity of staying wirelessly connected grows, the 2014 Honeywell survey affirms that fliers expect constant and speedy Wi-Fi when traveling. The research was conducted by Kelton among more than 1,000 adults in the United States who have used Wi-Fi on planes within the past 12 months.


“You can pack your own meals, but you can’t pack your own Wi-Fi,” said Jack Jacobs, vice president, Marketing and Product Management, Honeywell Aerospace. “The commercial aviation industry has to pay attention to meet the demands of passengers, giving them the freedom to stay connected whenever and wherever they want. Honeywell’s survey affirms that consumers are accustomed to easy access to Wi-Fi, and they expect it to be fast and consistent like at home or work. Those expectations are expanding up into the sky.”


Connectivity is Crucial
The results also indicate that fliers believe wireless connectivity should always be a part of the in-flight experience, and it may even be viewed as a necessity:


  • In-flight Wi-Fi availability influences flight selection for 66 percent of passengers. 
  • Nearly one in four (22 percent) admitted they’ve paid more for a flight with Wi-Fi, and close to one in five (17 percent) have switched from their preferred airline because another carrier had better Wi-Fi offerings.
  • Demand is so strong that 37 percent would be upset if they didn’t have Wi-Fi access on their next flight, which is about the same amount (35 percent) as those who would be disappointed about not having food or drinks available for purchase. 
  • Eighty-five percent would use Wi-Fi on most or all flights if it was free.


Sacrifice for Speed
Constant accessibility is key, but passengers also desire fast connections that enable them to stream videos, live chat with friends and family, and download files quickly. Almost half the respondents would be willing to experience a travel-related inconvenience for Wi-Fi that’s as fast as it is at home. From this group:


  • Over two in five (45 percent) of these people would endure airport security twice.
  • More than one in three (34 percent) would show up three hours before boarding time for superior speed.
  • Twenty-nine percent would even swap their ticket to fly standby on a plane with Wi-Fi that’s as fast as it is at home.


Fun with Wi-Fi
The Honeywell survey results asserted that air passengers demand constant and speedy Wi-Fi and also explored why passengers desire it so much. Consistent connectivity can enable productivity, entertainment and a little bit of fun: 


  • Thirty-nine percent received personal or general breaking news in-flight.
  • Close to one in five (19 percent) have used in-flight Wi-Fi to plan their next vacation.
  • Nine percent of respondents pretended they were in the office while on vacation.

Fliers are keeping themselves entertained onboard with Wi-Fi and, interestingly, the survey found that over half (54 percent) say they would be embarrassed if an in-flight neighbor saw what they were doing for fun, including: 


  • Fifty percent would be embarrassed if someone saw them perusing a dating site.
  • Thirty-two percent would be embarrassed if they were caught watching cat videos.
  • Thirty percent would not want to be seen watching children’s movies.


Staying Connected with Honeywell
Honeywell’s industry-leading connectivity product portfolio caters to customers’ needs from the cockpit to the cabin. As demand for fast in-flight connectivity continues to grow, Honeywell has built a focus on providing a comprehensive portfolio of products and services, whether it is air-to-ground, L-band or GX Ka-band solutions, to meet the needs of regional and global customers. Honeywell’s connectivity products have the largest air transport installed base and are onboard almost every aircraft with current broadband solutions. Honeywell is well-positioned to bring together its connectivity experience with proven systems integration to deliver the most expansive, consistent, high-speed connectivity network in the world.


About The Survey
The Honeywell Aerospace Wi-Fi Survey was conducted between June 6 and June 19, 2014, among 1,045 Americans age 18 and over who have used in-flight Wi-Fi in the last 12 months, using an email invitation and an online survey by Kelton, a leading global insights firm. Results of any sample are subject to sampling variation. The magnitude of the variation is measurable and is affected by the number of interviews and the level of the percentages expressing the results. In this particular study, the chances are 95 in 100 that a survey result does not vary, plus or minus, by more than 3.0 percentage points from the result that would be obtained if interviews had been conducted with all persons in the universe represented by the sample. The margin of error for any subgroups will be slightly higher.


Supporting Resources


Thousands of Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft worldwide. The Aerospace business unit develops and integrates technologies that span air traffic modernization, flight and runway safety, engines, cockpit and cabin electronics, connectivity, logistics and more that deliver safe, efficient, productive and comfortable transportation-related experiences. For more information, visit or follow us at @honeywell_aero on Twitter.


Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London and Chicago Stock Exchanges. For more news and information on Honeywell, please visit


# # #


Media Contacts:
Gwennie Cheung
Honeywell Aerospace
+1 (646) 589-1741

Steve Brecken
Honeywell Aerospace
+ 1(602) 365-2347


Honeywell Aerospace Media Center



  Back to Index Top