Press Releases
  Back to Index  
Text Size:  
Honeywell Pumps Up Energy Savings At California’s East Valley Water District 


Infrastructure Improvements and Utility Program Participation Expected to Save More Than $520,000 in Annual Energy Costs

MINNEAPOLIS, Feb. 12, 2014 – Honeywell (NYSE:HON) today announced it will be working with East Valley Water District (EVWD) of Highland, Calif., to improve water distribution systems and reduce utility costs through a combined energy conservation and automated demand response (ADR) program. The project is the first of its kind among municipal water authorities nationwide and, when complete, is expected to reduce annual energy costs by $523,000.


The project will be financed through a 10-year, $4-million energy performance contract
with Honeywell, allowing the water district to pay for the upgrades through the anticipated savings, which the company guarantees. As a result, the program should provide the needed improvements without requiring EVWD to invest upfront capital.

The local electric company, Southern California Edison (SCE), will also provide a $500,000 rebate for the district’s involvement in the ADR program, which requires EVWD to trim energy use on days when the call for electricity puts significant stress on the utility grid.

“As a water district, we are pleased to have the opportunity to dramatically reduce our energy use, help our state reach its energy reduction goals and increase system efficiencies for our customers,” said John Mura, CEO and General Manager for East Valley Water District. “We take pride in being environmental stewards; this project can help us better manage our water system while reducing greenhouse gas emissions.”

According to a 2005 report by the California Energy Commission, 19 percent of the state’s energy requirements and about 30 percent of natural gas consumption is water related, including water treatment, and pumping and delivery, among other activities. EVWD’s efforts and similar projects could have a considerable impact on the state-wide goal to reduce greenhouse gas emissions 20 percent by 2020.

“Opportunities to reduce emissions and energy use are not limited to large commercial
and industrial operations, or public facilities,” said Paul Orzeske, president of Honeywell Building Solutions. “Water and wastewater operations can realize tremendous savings through upgrades as well. Honeywell can help these organizations optimize their systems and dedicate fewer resources to electricity and natural gas.”

As part of the program, Honeywell will improve the district’s infrastructure by replacing older, inefficient water pumps with high-efficiency models and modifying pumping schedules so water reserves are replenished only during off-peak utility hours.

Energy rates are typically highest from 1 p.m. to 5 p.m. daily. During those times, EVWD will automatically shut down the majority of its pumping stations to reduce operating costs, while relying on stored water and a few key stations to continue to provide uninterrupted service to its 94,000 customers. In addition, EVWD is transitioning to a new electrical rate structure with SCE that provides incentives for off-peak consumption.

Honeywell will also upgrade outdated electrical switches and breakers at two facilities, and install an emergency generator at another to provide backup power in the event of a disruption.
The water district will further benefit by participating in the SCE ADR program. When the utility is facing a supply-demand imbalance or an overburdened grid, EVWD has agreed to automatically shed electrical load by further reducing the amount of pumping stations in use — without impacting service to customers.

Water stored in elevated tanks will be used to meet the needs of the district’s customers,
and facility personnel can opt out of a demand response event if reserves are low or full capacity is needed due to an emergency. The same controls that manage pumping schedules will be able to coordinate the ADR-related changes as well. And, when it’s time to make the adjustments, the controls will receive a signal from Honeywell’s Akuacom Demand Response Automation Server, which SCE uses to communicate with facility systems at participating customer sites.

A global leader in energy-saving technology and services, Honeywell has completed more than 5,000 energy-efficiency projects around the world, which includes work for water utilities across the United States and in the Caribbean. These projects are guaranteed to deliver more than
$5 billion in energy and operational savings. For more information, follow @HoneywellBuild on Twitter or visit Honeywell Building Solutions on the Web.


For more information about East Valley Water District visit the official website at

Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit

This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.


Aaron Parker

763-954-4257 (office)

763-607-6108 (mobile)


Mark Hamel 
763-954-6070 (office) 
952-334-4337 (mobile)

  Back to Index Top