Developed in China, the resins are tailored for fishing applications and ease of use in manufacturing
SHANGHAI, May 17, 2011 -- Honeywell (NYSE: HON) Resins and Chemicals announced today it has expanded its line of Aegis® nylon 6 resins to include a new formulation specifically tailored for fishing line and net applications.
This new formulation, Honeywell Aegis H95XC Gen II Resin, is designed to maximize transparency, flexibility, strength and elongation, which are key attributes needed in fishing line and nets. The resin also has critical performance additives already imbedded, allowing manufacturers to avoid the time and cost normally associated with blending the materials themselves to achieve the best results.
Honeywell developed the new resin at its technology center in Shanghai, China, working closely with local manufacturers that convert nylon or copolymer resin into filaments and fibers used to produce fishing lines and nets.
“This resin was developed based on the input of customers to achieve the combination of attributes they require and the ease of use in manufacturing they need,” said Jay Tang, marketing development manager for Honeywell Resins and Chemicals in China. “It is another example of our continuing efforts to customize resins to meet specific needs of our customers.”
Fishing lines and nets require certain attributes from nylon, including: transparency so the net cannot be seen underwater; flexibility or softness so the net and line are easy to handle, spread, fold and store; strength so the line or net does not break under heavy loads; and elongation to prevent knot slippage. Honeywell researchers used new proprietary quantitative testing methods for transparency and softness in formulating the resin to measure and prove its performance.
The company is currently sampling customers and plans to enter full production of the resin in the third quarter of this year.
Honeywell Resins and Chemicals is one of the world’s largest producers of nylon resin and caprolactam, a critical feedstock used for nylon production. Its resins are used in diverse applications such as fibers and filaments for carpeting, fabrics, nets and cords; engineered plastics components for automotive, consumer, and industrial applications; and films for food and protective packaging. Resins and Chemicals offers more than a half-century of technology and customer-focused application development expertise to enable sustainable growth worldwide.
Resins and Chemicals also produces chemical intermediates and is one of the world’s largest producers of ammonium sulfate fertilizer.
Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.
Media Contacts:
United States
Peter Dalpe
+ 1 973-455-4908
peter.dalpe@honeywell.com
Europe, Middle East, Africa
Martin Orsag
+42 02 4244 2279
martin.orsag@honeywell.com
Asia-Pacific
Judy Wang
+86 21 2894 2252
judy.x.wang@honeywell.com