First Air Demonstration Team to Use Alternative Fuels Will Fly Using Honeywell Green Jet Fuel Made from Camelina
DES PLAINES, Ill., May 20, 2011 -- UOP LLC, a Honeywell (NYSE: HON) company, announced today that Honeywell Green Jet Fuel™ will power two Air Force F-16 aircraft as part of a Thunderbirds demonstration at Joint Base Andrews in Maryland.
During a Joint Services Open House at the base on May 20 and 21, two Thunderbird aircraft will perform using a 50/50 blend of Honeywell Green Jet Fuel made from camelina and petroleum-based jet fuel. Camelina, grown and harvested for the Air Force by Sustainable Oils LLC, is an inedible, second- generation plant source for biofuels that does not deplete valuable food, land or water resources. This event will mark the first use of an alternative fuel blend by an air demonstration team.
To date the Air Force has fully certified Honeywell Green Jet fuel on the C-17 Globemaster III the F-16 and successfully demonstrated the fuel on the A-10 Thunderbolt, the F-15 Eagle and the F-22 Raptor platforms.
Honeywell UOP produced 400,000 gallons of Green Jet Fuel from sustainable, non-food sources for the Air Force as part of a joint program for the U.S. Defense Logistics Agency -- Energy (DLA-E) for alternative fuels testing and certification. The final fuel delivery under this program took place in early May 2011.
"The Air Force has clearly shown its commitment to diversified sources of energy through biofuels testing and certification," said Jim Rekoske, vice president and general manager of Renewable Energy and Chemicals for Honeywell's UOP. "We are proud to have successfully supported each of these efforts and that the Thunderbirds can continue their superior legacy using our Green Jet Fuel."
The Air Force held its first demonstration flight with Honeywell Green Jet Fuel in an A-10 Thunderbolt II in March 2010. It expects to achieve fleet-wide certification by 2013.
Honeywell UOP was the prime contractor or subcontractor on DLA-E contracts to produce almost 600,000 gallons of renewable jet fuel for the U.S. Navy and Air Force in October 2009. Working with feedstock partners Sustainable Oils, Solazyme and Cargill, Honeywell UOP process technology was used to produce 190, 000 gallons of fuel for the Navy and 400,000 gallons for the Air Force from animal fats, algae and camelina.
Honeywell UOP's Green Jet Fuel process technology was originally developed in 2007 under a contract from the U.S. Defense Advanced Research Projects Agency ( DARPA) to produce renewable military jet fuel for the U.S. military. The process is based on hydroprocessing technology commonly used in today's refineries to produce transportation fuels. It produces an aviation biofuel that can be blended seamlessly with petroleum-based fuel. When used as part of as much as a 50 percent blend with petroleum-derived jet fuel, Green Jet Fuel is a drop-in replacement that requires no changes to the aircraft technology and meets all critical specifications for flight.
Honeywell's UOP, a recognized global leader in process technology to convert petroleum feedstocks to fuels and chemicals, is developing a range of processes to produce green fuels from natural feedstocks. In addition to its Green Jet Fuel process technology, the company has commercialized the UOP/Eni Ecofining™ process to produce Honeywell Green Diesel™ from biological feedstocks. It also has a joint venture with Ensyn Corp. in Envergent Technologies LLC, which offers pyrolysis technology for the production of renewable heat, power and transportation fuels.
UOP LLC, headquartered in Des Plaines, Illinois, USA, is a leading international supplier and licensor of process technology, catalysts, adsorbents, process plants, and consulting services to the petroleum refining, petrochemical, and gas processing industries. UOP is a wholly-owned subsidiary of Honeywell International, Inc. and is part of Honeywell's Specialty Materials strategic business group. For more information, go to www.uop.com.
Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
Media Contact:
Susan Gross
+1 847-391-2380
susan.gross@honeywell.com