• New Renewable Energy Facility Will Cut Costs, Create Jobs and Power Local Wastewater Plant
• City-wide Initiative Will Help Wilmington Trim Its Carbon Footprint by Approximately 35 Percent
MINNEAPOLIS, Sept. 12, 2012 – Honeywell (NYSE:HON) today announced a $35-million renewable energy project for the City of Wilmington, Del., which will feature a
first-of-its-kind facility that converts two sources of biogas into power and heat for the city’s wastewater treatment plant.
The project is part of a city-wide initiative to decrease energy costs and greenhouse gas emissions, a program that has also included Honeywell-led solar installations and energy-efficient building improvements. Combined, the upgrades will help the city trim its carbon footprint by approximately 35 percent and meet nearly 50 percent of its electricity needs with renewable energy.
The efforts are also helping produce and sustain local jobs. Honeywell plans to use Wilmington-area contractors and union labor to support the latest work, providing more than 100 jobs during construction and creating up to five permanent positions.
In addition, Wilmington has been able to make these energy- and environmental-focused improvements without increasing budgets or taxes. City officials intend to use the subsequent reduction in utility and operating costs, savings that are guaranteed through performance contracts with Honeywell, to fund the upgrades and ongoing support. In addition, the work is expected to deliver savings beyond the money required to finance the activities.
“The City of Wilmington continues to position itself as a leader in municipal sustainability,” said Mayor James M. Baker. “By working with Honeywell to build the renewable energy facility and make a variety of other unique, innovative improvements across the city, we can significantly reduce energy consumption and greenhouse gases without extra funding from taxpayers.”
The centerpiece of the new project is the construction of a Renewable Energy Biosolids Facility to harvest and harness naturally occurring biogas, supplying a renewable resource to not only generate electricity for the Hay Road Wastewater Treatment Plant, but provide thermal drying to greatly reduce the volume of sewage sludge the city pays to remove.
The biosolids facility will capture methane produced by anaerobic digesters at the Hay
Road plant, a potential energy source that is currently flared off. The gas will mix with additional methane from the nearby Cherry Island Landfill, which is operated by the Delaware Solid Waste Authority. And the blend will be purified at the facility and used to power reciprocating engines that can generate up to 4 megawatts of electricity, enough energy to provide up to 90 percent of the treatment plant’s power.
The biosolids, or sewage sludge, that come out of the digesters will also be dehydrated by heat recovered from the engines. This thermal drying process is expected to reduce the amount of sludge the city needs to truck away by approximately 75 percent — from 140 to 35 tons per day — greatly reducing material-handling costs.
The biosolids facility is also projected to trim greenhouse gas emissions by 15,700 metric tons annually. According to figures from the U.S. Environmental Protection Agency, the decrease is equivalent to removing more than 3,000 cars from the road.
“Municipalities face the unique challenge of managing utility costs and emissions while simultaneously keeping taxpayer obligations in check,” said Paul Orzeske, president of Honeywell Building Solutions. “Through Honeywell’s expertise and the security of a performance contract, Wilmington can make necessary investments to further its environmental stewardship without adversely impacting its bottom line.”
Construction of the Renewable Energy Biosolids Facility is expected to begin in spring of 2013 and the building will be commissioned in summer of 2014. Honeywell is collaborating with engineering firm CH2M HILL to design the project. The company will also provide operations and maintenance support for the facility through an annual service agreement.
This is the second phase of the city’s sustainable energy initiative, building on previous work performed by Honeywell that includes the installation of photovoltaic solar arrays at the Wilmington water filtration plant and municipal complex, conversion of all traffic lights to high-efficiency light-emitting diodes, and the installation of ultra-efficient lighting, heating and air-conditioning equipment in city-owned properties. To date, the project has generated more than $1 million in energy cost savings, and $590,000 in rebates and renewable energy credit revenue.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywell.com.
This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.
Media Contact:
Aaron Parker
Honeywell
763-954-4257
aaron.parker@honeywell.com