Overwhelming evidence gathered by collaborative auto industry processes has demonstrated new low-global-warming offering can safely be used in automobiles
MORRIS TOWNSHIP, N.J., Dec. 14, 2012 – Honeywell (NYSE: HON) today said it is confident that SAE International, recognized as the world’s leading automotive engineering association, will reconfirm that HFO-1234yf, Honeywell’s new low-global-warming-potential automotive air conditioning refrigerant, is safe for use in automobiles.
SAE International, in announcing an update on its fourth and latest Cooperative Research Project (CRP) on the refrigerant, said, “To date, the majority of the OEMs involved in the new CRP do not believe that any of the new information reviewed will lead to a change in the overall risk assessment.”
“With the exception of Daimler, no OEM in the CRP has provided information that would suggest a concern for the safe use of R-1234yf in their vehicles,” SAE International said.
“Based on today’s announcement, Honeywell continues to believe that SAE International’s latest evaluation will only reconfirm the overwhelming body of data – including rigorous and comprehensive studies conducted in Europe, the U.S. and Japan – that have clearly and repeatedly determined that HFO-1234yf is safe for use in automobiles,” said Dr. Ian Shankland, chief technology officer for Honeywell Performance Materials and Technologies. “HFO-1234yf is a safe and effective refrigerant, and it is better for the environment.”
SAE International, formerly known as the Society of Automotive Engineers, is an independent, global association of more than 133,000 engineers and related technical experts in the aerospace, automotive and commercial-vehicle industries. Previously, HFO-1234yf was the subject of comprehensive testing conducted over a three-year period under an SAE International CRP using proven, standard methods for evaluating new products and materials in automobiles. That CRP, which was sponsored by 15 global automakers, including all leading German automakers, concluded that HFO-1234yf is safe for use in automobile applications.
HFO-1234yf is a highly efficient, low-global-warming refrigerant that was developed as a direct replacement to HFC-134a in mobile air-conditioning applications. Compared with HFC-134a, HFO-1234yf offers a 99.7 percent improvement in global warming potential and far exceeds the European Union Mobile Air Conditioning (MAC) Directive requirement.
Under rare conditions, HFO-1234yf exhibits mild flammability, at levels significantly lower than highly flammable materials already present under the hood of an automobile, including motor oil, automotive transmission fluid, radiator antifreeze, brake fluid, and compressor lubricant – not to mention fuel. For a video on this topic, which includes a comparison of HFO-1234yf vs. HFC-134a and other materials, visit www.1234facts.com/resources or www.1234fakten.de/ressourcen.
SAE International’s previous research projects have addressed the issue of flammability, employing proven and universally accepted fault-tree risk assessment techniques to evaluate the real-world possibility of a fire and human impact. SAE International said in its latest statement that it has expanded its fault-tree assessment in the new CRP to “ensure that newly-identified information and testing from each of the OEMs is incorporated.”
As part of SAE International’s programs, internationally recognized laboratories – including Hughes Associates Inc. and France’s Institute National de l’Environment Industriel et des Risques (INERIS) – conducted extensive testing on flammability and safety, and all concluded that HFO-1234yf is safe for use in automobiles.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.
Contacts:
Media
Peter Dalpe
(973) 455-4908
peter.dalpe@honeywell.com