Press Releases
  Back to Index  
Text Size:  
Honeywell’s UOP Technology Selected To Clean Offshore Natural Gas In The United Kingdom 


Gas treating technology includes first membrane-based system on a Floating Production, Storage and Offloading (FPSO) vessel in the North Sea


DES PLAINES, Ill., Aug. 19, 2014 -- UOP LLC, a Honeywell (NYSE: HON) company, announced today that it has been selected by BW Offshore to remove contaminants from natural gas aboard a new Floating Production, Storage and Offloading (FPSO) vessel off the coast of Scotland.


The vessel, which will be leased to Premier Oil, will include a UOP SeparexTM Membrane System to remove carbon dioxide. While the technology has been successfully used elsewhere, this will be the first FPSO in the North Sea to use a membrane-based treatment system. UOP guard bed adsorbents will also be used to remove mercury and hydrogen sulfide. These contaminants must be removed to meet export and end-user specifications, and to protect downstream equipment.


Vast quantities of recoverable natural gas lie under the Earth’s oceans. Accessing, treating and recovering these natural resources can be challenging due to ocean movement, environmental regulations, and space and resource constraints on offshore production facilities. 


“UOP is continually innovating to create lightweight, compact, chemical-free equipment that is ideal for the complex offshore gas environment,” said Rebecca Liebert, senior vice president and general manager of Honeywell’s UOP Gas Processing and Hydrogen business unit. “By integrating UOP Separex membrane technology and guard bed adsorbents into a single system, we are able to create a solution that improves gas processing efficiency while reducing operating costs for FPSO operators.”


Scheduled for start-up in 2017, BW Offshore’s FPSO will be located approximately 125 miles east of Aberdeen, Scotland, in the Catcher oil field, in which Premier Oil has a 50 percent operating interest. It will have a processing capacity of 60,000 barrels per day of oil and a storage capacity of 650,000 barrels.


UOP Separex technology upgrades natural gas streams by removing carbon dioxide and water vapor. These contaminants must be removed to meet the quality standards specified by pipeline transmission and distribution companies as well as natural gas end users. Decades of operation in natural gas service have demonstrated that Separex membranes are the most robust for natural gas service and can achieve the longest membrane life in the industry. They eliminate the need for solvents, which could spill and damage the marine ecosystem. To date, more than 130 of UOP’s membrane systems have been installed worldwide.


UOP guard bed adsorbents allow the removal of trace amounts of sulfur or mercury. These high-loading metal oxide adsorbents provide reliable protection for downstream equipment and consistently meet pipeline gas specifications, with no moving parts and no operator intervention.


Honeywell offers a broad range of technologies for natural gas production, processing and transportation. Its UOP Gas Processing and Hydrogen business has supplied technology to more than 3,600 individual process units for gas processing in a broad range of applications throughout the world. The business offers technology, equipment and materials to treat and process natural gas, and to purify hydrogen used in refineries. Its gas technologies extract contaminants such as water, mercury, sulfur and carbon dioxide from raw natural gas. UOP also offers technologies to recover natural gas liquids (NGLs). UOP gas processing solutions are offered as efficient pre-engineered equipment packages or licensed technology.


Honeywell Process Solutions provides advanced automation, monitoring, safety and security systems for the entire gas supply chain to help operators increase plant reliability and efficiency, while reducing costs and risk.


BW Offshore is a leading global provider of floating production services to the oil and gas industry. BW Offshore is the world’s second largest contractor of its kind with a fleet of 14 FPSOs and one Floating Storage and Offloading unit represented in all major oil regions worldwide.


Premier Oil plc is a leading independent exploration and production company with oil and gas interests in the North Sea, South East Asia, Pakistan and the Falkland Islands, as well as exploration interests in Brazil, Iraq and Kenya.


UOP LLC ( is a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries. UOP is a wholly-owned subsidiary of Honeywell International Inc. and is part of Honeywell’s Performance Materials and Technologies strategic business group, which also includes Honeywell Process Solutions, a pioneer in automation control, instrumentation and services for the oil and gas, refining, petrochemical, chemical and other industries.


Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges.  For more news and information on Honeywell, please visit


This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.



Krystal McMiller

(847) 391-3561

  Back to Index Top