Press Releases
  Back to Index  
Text Size:  
Honeywell’s UOP Technology Selected To Boost Yields At Romania’s Largest Synthetic Rubber Facility 

Honeywell’s UOP KLP™ process maximizes yields for synthetic rubber production while eliminating unwanted byproducts

DES PLAINES, Ill., Aug. 7, 2012 -- UOP LLC, a Honeywell (NYSE: HON) company, announced today that its technology has been selected to boost yields at Romania’s largest synthetic rubber production facility.


Romania’s Energy Bio-Chemicals will use Honeywell’s UOP KLP™ process to purify butadiene, a monomer used to produce synthetic rubber, at the company’s CAROM Onesti Styrene Butadiene Rubber facility. The project is part of the company’s modernization investment program to upgrade their butadiene installation and increase production.


Butadiene demand – driven by growth in the replacement tire industry, and electronics and consumer markets – exceeded supply by 170 thousand metric tons in 2011, according to the May 2012 Chemsystem Nexant report. Currently, Europe and the Middle East together are responsible for more than a quarter of the global butadiene demand. 

“UOP is committed to technologies that help refining and petrochemical producers maximize their yields,” said Pete Piotrowski, vice president and general manager of Honeywell’s UOP Process Technology and Equipment business unit. “As global demand for tires continues to grow, UOP’s technology allows producers to maximize yields with nearly 100 percent conversion of vinyl acetylene to butadiene.”


The KLP process increases the yield of butadiene, while also eliminating acetylene, a difficult-to-handle and unwanted byproduct, from the process. UOP will also provide a proprietary Caustic Merox unit to remove sulphur from the crude C4 feedstock. The contract includes licensing, engineering, technical support and catalysts.


Butadiene is a major petrochemical commodity used in the production of tires and other products in the automobile or appliance industry. Polymer-grade butadiene must be high purity and free of acetylenes, sulfur and other heavy components.


Honeywell’s UOP KLP process selectively adds hydrogen to acetylenes in a facility’s crude butadiene stream, typically providing an additional 1.5 to 2 percent increase in butadiene yields compared with alternative solvent removal methods not employing UOP’s KLP process.


In addition, elimination of the acetylenes typically provides a 1 to 3 percent increase in Raff-1 product yield. Raff-1 is another valuable byproduct of butadiene extraction processes, containing C4 olefins such as isobutylene and butene-1.


UOP’s process also enables safer operations by eliminating concentrated acetylene streams, which can become an explosion hazard. The KLP process can be used in new installations or in retrofit applications to increase product quality and yields by eliminating the costly first-stage extractive distillation step of two-stage butadiene extraction processes.


Currently, eight KLP units are in operation worldwide with a production capacity of more than 1 million metric tons annually.

UOP LLC, headquartered in Des Plaines, Illinois, USA, is a leading international supplier and licensor of process technology, catalysts, adsorbents, process plants, and consulting services to the petroleum refining, petrochemical, and gas processing industries. UOP is a wholly-owned subsidiary of Honeywell International, Inc. and is part of Honeywell’s Performance Materials and Technologies strategic business group. For more information, go to

Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit

This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

Krystal Hughes
(847) 391-3561

  Back to Index Top