Press Releases
  Back to Index  
Text Size:  
Honeywell’s Spectra Shield® Ballistic Material Selected To Improve Armor For U.S. Army Helicopters 


High-strength Spectra Shield material to better protect Black Hawk and Chinook helicopters and soldiers while also significantly reducing armor weight

MORRIS TOWNSHIP, N.J., Oct. 22, 2012 – Honeywell (NYSE: HON) announced today that its Spectra Shield® ballistic material will be used to improve armor protection on U.S. Army helicopters.

The Protective Group, Inc. (TPG), a leading developer and integrator of lightweight composite armor for military aircraft, is incorporating Spectra Shield material into armor upgrades for U.S. Army UH-60 Black Hawk and CH-47 Chinook helicopters.

“Spectra Shield material provides an ideal combination of proven ballistic performance and light weight, which is critical for applications ranging from body armor to aircraft,” said Roy Ash, global marketing manager for Honeywell’s Advanced Fibers and Composites business. “Armor that uses Spectra Shield material provides a superior level of protection for helicopters and the personnel inside, while the material’s lighter weight will allow the aircraft to carry heavier loads and save fuel.”

The new TPG solution is expected to reduce armor weight on the Black Hawk and Chinook helicopters by as much as 40 percent compared with the currently fielded system. TPG expects to upgrade armor on approximately 200 Chinook helicopters over the next four years under a contract from the U.S. Army, and is also working to meet the needs of the Black Hawk community.

TPG is an industry leader in developing survivability solutions for aviation platforms and the manufacturer of helicopter ballistic protection systems for the Special Forces and an increasingly larger percentage of the U.S. military’s helicopter fleet.

“Honeywell’s materials and expertise enabled us to deliver design solutions that meet the demanding specifications set out by the U.S. Army,” said Michael Breslin, executive vice president of business development for TPG. “The proven performance of Spectra Shield materials in military applications made it a superior choice for this integrated solution.”

Spectra Shield is a composite material made with Spectra® fiber, an ultra-high-molecular-weight polyethylene fiber that, pound for pound, is 15 times stronger than steel, yet light enough to float. Honeywell’s patented Shield technology lays parallel strands of synthetic fiber side by side and holds them in place with a resin system. Layers of the material are then cross-plied at right angles and fused into a composite structure under heat and pressure.

Honeywell ballistic materials have been trusted to protect military and police forces around the world for more than two decades. In addition to military aircraft, they are used in a variety of applications where lightweight strength is critical, including bullet-resistant helmets, vests, breast plates and combat vehicles.

Honeywell maintains an active Spectra fiber and ballistic materials research and development program focused on meeting increased demand for its high-performance materials.

Spectra fiber is also used in a wide variety of industrial and recreational applications, including rope and lifting slings, mooring lines, fishing line, sail cloth and security netting.

For more information, visit

Honeywell Performance Materials and Technologies is a global leader in developing and manufacturing advanced materials and process technologies. These materials and technologies are used by people every day in a wide range of industries and applications, from petroleum refining to environmentally friendlier refrigerants to bullet-resistant vests. Our advanced materials are critical in the manufacture of products ranging from nylon to computer chips to pharmaceutical packaging. Process technologies developed by our UOP business form the foundation for most of the world’s refiners, efficiently producing gasoline, diesel, jet fuel and petrochemicals. UOP is now pioneering technology to produce real fuels from renewable energy sources.


Honeywell ( is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit


This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.

Media Contact:
Nina Krauss

  Back to Index Top