Press Releases
  Back to Index  
Text Size:  
9/19/2013 
Honeywell’s Solstice® Liquid Blowing Agent Used In New, Highly Durable Roof For Cleveland Airport 

 

Spray foam system protects more than 500,000 square feet of roofing at Ohio’s largest and busiest airport; roof is rated to resist severe hail

MORRIS TOWNSHIP, N.J., Sept. 19, 2013 -- Honeywell (NYSE: HON) announced today that its Solstice™ Liquid Blowing Agent (LBA) has been selected as a key component in the spray foam roofing system for the Cleveland Airport System, including multiple terminal and maintenance buildings at Cleveland-Hopkins International and Burke Lakefront airports.

 
West Development Group, the LaGrange, Ohio-based company that developed the spray foam roofing system featuring Solstice LBA, will apply the spray foam to more than 500,000 square feet of roofing at the two airports. The system recently received a severe hail rating from FM Approvals, the testing and certification arm of FM Global, which is one of the world’s largest property insurers.


“The new spray foam roof was more cost-effective because we could apply it directly over our old roof, and it has helped us minimize disruption to passengers,” said Rob Henderson, Building Maintenance manager, Cleveland Airport System. “As a bonus, our insurance premiums are now lower because our insurer, FM Global, approved the roof components.”

Blowing agents such as Solstice LBA allow closed-cell spray foam insulation to expand and provide the majority of the foam’s excellent insulating properties. Closed cell spray foam is used for a variety of applications, including appliance and structural insulation, as well as roofing.


Solstice LBA is a next-generation blowing agent with a global warming potential of 1, significantly lower than previous-generation hydrofluorocarbon (HFC) blowing agents. Solstice LBA is nonflammable, has received EPA approval under the Significant New Alternatives Policy (SNAP) Program and is not a volatile organic compound.


“Solstice LBA has proven to be a superior blowing agent and a seamless drop-in replacement for the HFC-245fa blowing agent which we have used for years,” said Jack Moore, project manager, West Roofing Systems.


“Solstice LBA offers significant energy efficiency and climate impact benefits to building owners at costs that are comparable to or lower than other blowing agents,” said Laura Reinhard, Honeywell’s global product manager for spray foam blowing agents. “Around the world, customers in a variety of industries – from spray foam to appliance insulation – have responded extremely positively to this breakthrough blowing agent.”


In addition to Solstice LBA, Honeywell's family of Solstice-branded products includes stationary and mobile refrigerants, gaseous blowing agents, propellants, and solvents based on Honeywell’s new hydrofluoro-olefin technology that helps customers lower their carbon footprint without sacrificing end-product performance.


The products have been developed and are being commercialized by Honeywell’s Fluorine Products business, a leader in the manufacture and supply of zero ozone-depleting refrigerants used by top air-conditioning and refrigeration makers worldwide, and blowing agents for energy-efficient foam insulation, as well as hydrofluoric acid and precursors for nuclear fuel.


For more information on Solstice LBA, visit www.honeywell-solsticelba.com.

Honeywell Performance Materials and Technologies is a global leader in developing and manufacturing advanced materials and process technologies. These materials and technologies are used by people every day in a wide range of industries and applications, from petroleum refining to environmentally friendlier refrigerants to bullet-resistant vests. Our advanced materials are critical in the manufacture of products ranging from nylon to computer chips to pharmaceutical packaging. Process technologies developed by our UOP business form the foundation for most of the world’s refiners, efficiently producing gasoline, diesel, jet fuel and petrochemicals. UOP is now pioneering technology to produce real fuels from renewable energy sources.

Honeywell is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.

This release contains certain statements that may be deemed "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

Contact:
Jeannine Sohayda
(973) 455-2706
jeannine.sohayda@honeywell.com

  Back to Index Top